[Thông Báo] Cập Nhật Địa Chỉ Công Ty và Thông Tin Xuất Hóa Đơn VAT. Xem chi tiết
[Announcement] Update of Company Address and VAT Invoicing Information. See more
Container dollies are transport platform trucks where the container boxes can be stacked for transport or storage as is in factories, logistics warehouses, and the like that use container boxes. Four-wheel types are most common, but there are also 6-wheel types compatible with long container boxes and dolly types too. The platform truck's main body too can be stacked for storage. Materials they are made of are metals such as stainless steel and aluminum as well as resin, and materials can be selected according to the operating environment. With fixed types, container dolly sizes can be selected to fit the container boxes used. However, there are expandable types where the platform truck size can be freely adjusted and are compatible with container boxes of various sizes. There are also those with handles that are easy to transport and where noise reduction measures have been taken.